Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you cross a KAL style Mag-Gard breaker to PowerpacT?
Issue:
What is the PowerpacT equivalent to an KAL, KAP, or KAF style Mag-Gard MCP (motor circuit protector)?

Product Line:
Legacy KAL type circuit breakers

Resolution:
KA type Mag-Gard motor circuit protectors (MCPs) can be replaced by PowerpacT MCPs, but there are some important differences. These two families of breakers have different dimensions, connection points, and accessories. Because of this, the equipment they are installed in will usually require some modification and in some cases, replacement of the equipment will be necessary. Please see attached for the different dimensions.

NOTE: If the KAL is installed in an old KA individual enclosure, then the below H or J Frame PowerpacT WILL NOT WORK. It will require a brand new enclosure and a new thermal/magnetic breaker with 'instantaneous' adjustments and NOT just the Mag Guard MCP.

The best crosses for legacy KA type MCPs to PowerpacT MCPs are as follows:
LegacyPowerpacT
KAL3615026MHJL36150M74
KAL3625021MJJL36250M75
KAL3625022MJJL36250M75
KAL3625025MJJL36250M75
KAL3625026MJJL36250M75
KAL3625029MJJL36250M75
KAL3625030MJJL36250M75
KAL3625031MJJL36250M75
KAL3625032MJJL36250M75
KAL3625033MJJL36250M75


KAP  . . . crosses to JJP . . . or HJP . . .
KAP . . . MT crosses to JJM . . . or HJM . . .
KAF  . . . crosses to JJF . . . or HJF . . .
Existing handle operators will not work on the replacement breakers. For MCC applications, a new bucket will be required.

Schneider Electric Canada

Attachment(s)
KAL KCL Dimensions.pdf [85.96 KB]
Powerpact H and J Dimensions.pdf [2.75 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings