Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the elevating nuts for an NF interior ?

Issue:
Replacement leveling nuts for NF panelboard interiors

Product Line:
NF Panelboards

Environment:
Installation

Cause:
Replacement

Resolution:
The elevating nut for an NF interior is part number 80114-027-01.
These are supplied as standard on 400A panels and larger (Four are included). The elevating nuts are NOT included with 250A, or less interiors.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings