Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 8536 single phase starters physically a 2 Pole starter or a 3 pole starter wired as single phase?
Issue:
Checking if the 8536 single phase starters physically have a 2 Pole starter or a 3 pole starter wired as single phase.

Product Line:
8536 Starters

Environment:
NEMA Contactors and Starters

Cause:
Product feature and wiring.

Resolution:
The single phase unit is built on a three phase frame but is a true single phase starter.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings