Issue
What are the descriptions of the DNP function codes listed in the ION Meter DNP Device Profile Guides?
Product Line
Any PowerLogic ION meter such as:
ION 7330/7350
ION 7500/7600
ION 7550/7650
ION 8600
ION 8650
Environment
DNP Communications
Cause
DNP Function codes are listed in the ION Meter DNP Device Profile Guides without descriptions for each function code.
Resolution
Below is a table representing DNP function codes and their description:
In the PowerLogic ION8650 DNP 3.0 Device Profile technical note (70022-0126-00), the DNP Objects and the supported function codes are listed. This document is attached to this article.
By referring to the above table, it can be determined what each function code represents.
Released for: Schneider Electric Canada