Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I change the trip unit of the Powerpact H, J and L frame circuit breakers which are equipped with an I-Line jaw assembly for installation in I-Line panelboard and QED I-Line distribution sections?

Issue:
Change the trip unit of the Powerpact H, J and L frame circuit breakers for installation in I-Line panelboard and QED I-Line distribution sections

Product Lines:
Panelboards and Switchboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 29 and 94 -1989, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1, UL891

Cause:
Changing a trip unit, when possible, can be less costly and more convenient than obtaining a new circuit breaker.

Resolution:
No, the presence and necessity of the mounting foot on the I-Line version of these circuit breakers excludes the capability of changing the trip unit.
This is the case for thermal-magnetic versions as well as versions with Micrologic trip units.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings