How can we help you today?

What is the load requirement of a breaker communications module (S64205)?

Product Line:
Powerpact, Compact NS breakers, Powerlogic

Resolution:
Power requirements are 30 mA, 24 Vdc.

For information about the units, please consult the PowerPact™ M-, P- and R-Frame, and Compact™ NS630b–NS3200 Circuit Breaker 0612CT0101.


Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: