How can we help you today?

Are the 9001KS selector switches available with a metal knob?

Issue:
To find out if the 9001KS series of selector switch have a metal knob option

Product Line:
Push Buttons and Operator Interface

Environment:
9001KS selector switches

Resolution:
Metal selector switch knobs are no available, only plastic. The metal and plastic difference on the 9001K and SK operators are for the bezel and not the knob itself.