Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do we interlock push buttons on a XACA** pendant station?

Issue:
What is the part number for an interlocking device for push buttons in a XACA pendant station?

Product Line:
XACA pendant stations

Environment:
XACA 22mm pendant stations

Cause:
Push buttons need to be interlocked so both push buttons can not be pushed at the same time.

Resolution:
An XACA009 mechanical interlock can be used with the booted push button operators, XACA941*, so you cannot depress both buttons at the same time.  This mounts to the metal plate in the middle of the pendant.   See attached exploded view.

Schneider Electric Canada

Attachment(s)
9001CT0001 BW, SKYP, XACA pendants.pdf [323.46 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings