Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we offer a padlock attachment for a 9001KR9R that doesn't hold the button depressed?

Issue:
Customer wants a padlock attachment for a 9001KR9R that doesn't hold the button depressed.

Product Line:
9001K/ 9001KS

Environment:
9001K/ 9001KS 30mm operators emergency stop

Cause:
For a particular application, the E-stop needs to be locked out to prevent being accidental engaged.

Resolution:
Schneider Electric does not offer a padlock attachment that will not hold an e-stop in the depressed position.  The emergency stop button needs to be accessible to push in case of emergency.  The only option Schneider electric can offer is a guard that will protect the button against accidental operation.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings