Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a guard for the 22 mm non trigger action emergency stop operators?
Issue:
Is there a guard for 22 mm push button that is not trigger action, such as the XB4BT42, XB4BS542, XB4BS142, XB5AT42, XB5AT542, and XB5AS142?

Product Line:
22 mm XB4 and XB5 emergency stop push buttons

Environment:
22 mm emergency stop push buttons

Cause:
Need to guard a 22 mm emergency stop push button that is not trigger action

Resolution:
We can use the standard metal guards that we use for the trigger action emergency stops.
Because the trigger action emergency stop is 5 mm taller than the non-trigger action devices the padlock function will not work but they can still be used to guard the emergency stop operator.
A ZBZ1600 can be used for the chromium plated guard, ZBZ1602 for a black guard, ZBZ1604 for red, ZBZ1605 for yellow, and ZBZ1606 for blue.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings