Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How does the Repeat Cycle work for a 9050JCK70V20 Timing relay?

Issue:
Repeat Cycle function for a 9050JCK70V20 Timing relay.

Product Line:
General Purpose JCK plug-in timers

Environment:
Square D plug-in timers

Resolution:
The 9050JCK70 Repeat Cycle timing Mode works when control power is applied to the coil. The Off time begins. At the end of the Off time, the output contacts energize and the On Time begins. At the end of the On Time, contacts de-energize and Off Time begins. This sequence continues until control power is removed from the coil. The 905JCK70 Timer can only have the same time intervals of Off and On times.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings