Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the XB7 line of operators, replacing the XB4 and XB5 lines?

Issue:
Are the XB4 and XB5 lines being replaced?

Product Line:
XB7

Environment:
XB7 22mm push button operators

Cause:
Clarify the purpose of the XB7 line, when XB4/XB5 already exist.

Resolution:
No.  The XB7 is a monolithic line of operators.  They have no replacement parts and are more economical than the other lines of operators.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings