How can we help you today?

What is XB4 LED service life?

100 000 hours.

Issue:
All specifications of XB4/XB5 product are not published in Digest 176; customers are unsure where to find additional specification and rating information.

Product Line:
All XB4/XB5 product

Environment:
US product

Cause:
Customers are unsure where to find specification and rating information if it is not in Digest 176

Resolution:
They are listed at 100,000 hours life.  Additional information can be found on the spec sheets for the individual light modules.  See attached example.

Schneider Electric Canada

Attachment(s)
Harmony XB4_ZB4 Metal Push Buttons_ZBVB4.pdf [116.24 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors