Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a rotary handle for a 2 pole Powerpact H frame circuit breaker?
Issue:
Rotary Handle for 2-pole H frame
Product Line:
Powerpact Molded Case Circuit Breakers
Resolution:
The rotary handle is only for the 3 pole module version of the H frame breaker. It will not work on HG and HD 2 pole versions, but it will work on 2 pole HJ and HL, as they are built with a 3 pole module.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings