Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When should we use rectangular versus round cover mounted control units for NEMA contactors and starters?

Issue:
When selecting a cover mounted control unit (such as HOAs, pilot lights, and push buttons) for NEMA contactors and starters when should we use square/rectangular control units and when should we use round control units

Product Line:
NEMA Contactors and Starters

Environment:
All NEMA Contactors and Starters

Cause:
Selecting the correct cover mounted control unit for NEMA Contactors and starters.

Resolution:
Square/rectangular mounted control units are for use in the pre-series K NEMA type 1 enclosed starters and contactors. Series K and later NEMA type 1, 3R, 4, 4X, and 12 use the round operators. Series K was introduced in 11/2010.


Keywords
9999SP28R, 9999SP2R, 9999SP3R, 9999SP4R, 9999SP5R, 9999SP12R, 9999SP13R, 9999SP14R, 0000SP15R, 9999SA2, 9999SA3, 9999SA10, 9999SC2, 9999SC8, 9999SC9, 9999SPL28R, 9999SPL28G, 9999SP29R, 9999SPL29R, 9999SPL29G

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings