How can we help you today?

How many pins do the RE48 timers have?

Issue:
How are configured the pins on the RE48 timing relays?

Product Line:
RE48 timers

Environment:
RE48 timers

Cause:
Identifying the pins on the RE48 timers

Resolution:
The RE48AML12MW, RE48ACV12MW all have 11 pins.

The RE48AMH13MW, RE48ATM12MW all have 8 pins.

For timing diagrams see each datasheet

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: