Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
9007 EQ1488 is obsolete. Do we have something to replace it?
Issue:
9007 EQ1488 replacement

Product Line:
Limit Switches

Environment:
Class 9007 EQ limit switches

Cause:
Need to replace a 9007EQ1488 limit switch.

Resolution:
The 9007AO105 may be used in its place.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings