How can we help you today?

Is there a through the door operating mechanism for the GV3P manual starters?

Issue:
GV3P Through the door mechanisms options

Product Line:
IEC Contactors and Starters

Environment:
GV3P Manual Starters and Protectors

Cause:
Product selection/feature

Resolution:
There are three different through the door operating mechanisms for the GV3P. There is the GV3APN01 which is rated
NEMA 1 and 12 in black with trip indication; the GV3APN02 which is also NEMA 1 and 12 in red/yellow with trip indication,
and the GV3APN04 which is NEMA 4/X red/yellow without trip indication.