How can we help you today?

What standard does the plug used on the EVlink station meet? What cars will it work with?

Issue:
What connector is used on the EVlink charging station?

Product Line:
PTEVC - ELECTRICAL VEHICLE

Resolution:
The EVlink Level 2 charging stations use the SAE J1772 type connector. The J1772 plug is rated NEMA 3S and is designed for indoor or outdoor use.
SAE J1772 Connector Front View J1772

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: