Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the force required to open and close the operating handle of a heavy duty safety switch?
Issue:
Handle force to turn a switch ON or OFF

Product Line:
Heavy Duty Safety Switch

Resolution:
The handle for required to turn a heavy duty safety switch on and off are as follows:
30 A, Series F = 7.6 lbs on; 6.5 lbs off
60 - 100 A, Series F = 9.7 lbs on; 8.3 lbs off
200 A, Series F = 15.7 lbs on; 16.8 lbs off
400 - 600 A, Series E = 36.2 lbs on; 33.0 lbs off
800 - 1200 A, Series E = 54.2 lbs on; 53.6 lbs off

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings