Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can one get a label to show a NQ or NF RTI panel is series rated?

Issue:
Series rating

Product Line:
Panelboards

Environment:
NQ or NF

Cause:
Application

Resolution:
A yellow and black label is included in the hardware bag that comes with the panel.
It can be filled out by the customer to note the tested series rating info in the digest or other recent spreadsheets . This label then can be affixed to the panel deadfront.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings