Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the minimum size terminal required for the QOU and QOUR breakers with ring terminations?
Issue:
What is the size of the terminal ring blade that will fit in a QOUR breaker?

Product Line:
Circuti Breaker

Resolution:
Use single UL Listed or CSA Certified insulated ring terminal or standard barrel tongue lug only. Must be suitable for 10-32 x 3/8 in. screw, provided. Tongue lug must be insulated.
NOTE: Some manufacturers’ terminals will be too wide to fit. Terminal ring blade must be under 0.44 in. (11.2 mm) wide.

Here is the instruction bulletin 48840-218-01.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings