Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there any branch breaker restrictions in a 400a Nema 3R NF panel ?

Issue:
Branch breaker restrictions for NF 400A N3R panels

Product Line:
Panelboards

Environment:
NF

Cause:
Selection

Resolution:
The largest true branch is 125a and sub-feed breaker is 150a.
Also 5 branches at 70a or more is a limit .

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings