Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I troubleshoot a residential EV charging station, EV230WS?
Issue:
An EV station is showing a detected fault indicator lamp lit.

Product Line:
PTEVC - Electrical Vehicle

Resolution:
The EVlink charging station detects several different types of faults. For residential (indoor) rated stations, the HMI (human machine interface) has 8 LED segments. Each of these segments, when lit red, indicates a different detected fault. Many conditions can be reset by powering the unit off by turning off the supplying 40 A circuit breaker.
Residential HMI Showing Segment 1 Detected Fault Lit
LED dial
EVlink Detected Faults
ResidentialDetected FaultAction
Segment 1 CCID system errorSee FA239096
Segment 2 Supply voltage errorVerify that the supply voltage between L1 and L2 is 208 to 240 VAC.
Segment 3 Main contact error (1)
Segment 4 Main contact error (2)
Segment 5 Vehicle requesting ventilationWait for call to cool.  Try charging again in 1 hour.
Segment 6 Invalid state
Segment 7Ground fault detected Unplug/re-plug vehicle
Segment 8Supply side ground not connected properlyWait for automatic reset or unplug/re-plug vehicle,  See FA268433

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings