Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Powerpact L-frame handle lock on and lock off devices?

Issue:
Padlock attachments for Powerpact L

Product Line:
PTCCB - MCCBS,EARTH LEAK&SWITCH

Resolution:
For removable, lock OFF only, part number S29370. Provisions for up to (3) padlocks. Instruction bulletin 48940-232-01.
For fixed, lock OFF only, part number NJPAF. Instruction bulletin 48041-046-02.
For fixed, lock ON or OFF, part number S32631. Instruction bulletin 48049-246-02.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings