Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the L600AWK suitable for use with the 4 pole L frame PowerPacT circuit breaker?
Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosure

Resolution:
No, only 3 pole circuit breakers can be used.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings