How can we help you today?

Can you padlock the breaker handle in an M800R enclosure?

Issue:
Can the operating handle of a circuit breaker in an M800R enclosure be padlocked?
Product Line:
M800R circuit breaker enclosure
Resolution:
The operating handle can be padlocked in the OFF position only by purchasing and field installing an S44936 handle padlocking device. The S44936 is considered a removable device. The operating handle can be padlocked in either the ON or OFF position by purchasing and field installing an S32631 handle padlocking device. The S32631 is considered a fixed device.

There is also an integral breaker cover on the enclosure that can be padlocked closed.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: