How can we help you today?

When attaching a PA, PH, PC, PX, or PE breaker to bus bars, what torque is required for the carriage bolts?

Product Line:
PA, PH, PC, PX and PE Circuit Breakers

Resolution:
There are 24 carriage bolts used to attach the above breakers to bus bars (4 bolts per pole, line and load).
The proper torque is 240 lb-in (27 N-m).
See below drawing as a reference.

Image showing the breaker and bolts

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category: