How can we help you today?

Is it possible to order an NQ factory assembled panelboard furnished with (42) QOB120CAFI?

Issue:
NQ factory assembled panelboard furnished with (42) QOB120CAFI

Product Line:
PTFDS - Final Distribution Enclosure Systems

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
Changes to requirements for arc fault protection of some circuits has resulted in greater need for CAFI branch breakers.  In the past a large proportion of these circuit breakers in an NQ panelboard necessitated a double panel.  This is no longer the case.

Resolution:
Yes, an engineering change now allows for (42) QOB120CAFI to be installed in a single section NQ panelboard.
The neutral pigtails of the branch breakers will be spliced as needed in order for the panelboard to accommodate all of the branch devices in a single section panelboard.

Schneider Electric Canada
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
Start your sales inquiry online and en expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings