Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the D9 suffix on the end of MH enclosure catalog number mean?
Issue:
With NQ, NF panel MH boxes, what does the D9 numbers represent

Product Line:
NQ and NF Panelboards

Environment:
Boxes - Enclosures

Cause:
Clarification-Product features

Resolution:
The D9 suffix option is for the box to be made  9" Deep vs the standard 5.75" Deep.
This option is standard in all Factory assembled 400A-600A NQ/NF Panelboard interiors with a Powerpact L 600A Frame Main breakers.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings