Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a HOM60120M200PC, Series S04 load center?
Issue:
Current design repair parts

Product Line:
Homeline load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Cover - HOMC60UC (the cover for the 60 space load center does NOT include a door, there is a door kit sold separately see below)
Cover Mounting Screw - 4020513002K
Interior Assembly - HOM60120M200PCI (Interior assembly does NOT include the main breaker, see below main breaker)
Neutral Bonding Screw - 4028345850K
Main Breaker - QOM2200VH
Door Kit - QOCDK60 (This is a separate door kit that attaches directly onto the front of the cover, but will only cover the area of the Deadfront Trim where the breaker handles are exposed. It Will NOT cover over the entire outer cover)
Directory label - 4026568602 (This is ONLY the part of the directory label that contains the circuit numbers and lines and is NOT the part that contains any of the text)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings