How can we help you today?

Does the Citect super genies need to be converted before tempalizing into the PES Global library?

Issue
Does the Citect super genies need to be converted before importing into the PES Global library?

Product Line
Ecostruxure Hybrid DCS

Environment
Ecostruxure Hybrid DCS, Windows 10 version 1902 (OS Build 18362.30), CitectSCADA

Resolution
The PES templatization process does not know about Super genie's. The Super genie is basically a pop up window or page that acts like a genie. The genies are used to call the super genies during run time. The templatization relies only on Genie's.  In order for the templatization to be successful, the Citect application must have Genie's.  Super genies, are part of Vijeo Citect process.  They do not play a role in PES. If the Citect application contains super genies or pop-ups, there is no need to convert them to genies before importing into the PES library.