How can we help you today?

Can the contactor be replaced on the Class 8536 Type SA Nema Size 00 starter ?

Issue:
8536 Starter, contactor replacement


Product line:
Starters, Type S


Environment:
Type S Full Voltage Contactors and Starters


Resolution:
Yes, the contactor can be ordered separately, make sure to use the same old nameplate after installing the contactor. Will use part number 8502*** using same voltage code concept. Customer will re-use mounting plate from 8536 starter that allows mounting of the overload relay