How can we help you today?

Do the EVlink Basic charging stations use any energy when in the standby mode? In other words, when no vehicle is being charged?

Issue:
What is the energy usage of the EVlink Basic charging station?

Product Line:
PTEVC - Electric Vehicles

Resolution:
The Evlink Basic draws less than 2 watts per charging port at an ambient temperature of 25 °C (77 °F) and a supply voltage of 240 Vac when not charging an electric vehicle.
In comparison to existing light bulb technologies;

EVlink Basic Power Comparison
DeviceWatts
EVlink Basic< 2
Incandescent Light Bulb60
Compact Fluorescent Bulb15
LED Lightbulb10


EVlink Basic Power Comparison

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: