Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will GFI, CAFI, and DF breakers function if the panel is a subpanel, instead of a main panel?
Issue:
Using GFI, CAFI, and DF breakers in main panel and subpanel application

Product Line:
Miniature Circuit Breakers, Load Centers

Resolution:
If the panel and breakers are wired correctly, it would not make any difference if the panel was a subpanel or a main panel. All electronic breakers (GFI, CAFI, DF, EPD, etc.) will work properly in both applications.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings