Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do safety switches have the option to add a receptacle?
Issue:
Do standard safety switches have the option to add a receptacle for regular plugs?

Product Line:
Safety Switches

Resolution:
The only receptacle options will be the Crouse-Hinds, Appleton, or Hubbellock that are factory installed only. No other receptacle options are available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings