Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Battery test on PTCC controllers
Issue
Does the PTCC controllers have battery testing feature

Product Line
PTCC controllers
Reclosers

Environment
Battery testing

Resolution
No, the PTCC controllers do not have an automated battery testing feature. But the PTCC controllers do have an alarm. The PTCC controllers monitors battery volts and if it is less than 24V(roughly) battery is indicated low.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings