Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the Form "E" mean for the 8536 type S starters?
Issue:
What does the Form "E" mean for the 8536 type S starters?

Product Line:
8536 Nema Starters

Environment:
Ordering

Cause:
Form E appears in the 8536 type S part number and clarification needed

Resolution:
The new form E adds an adaptor so that an IEC style bimetal overload relay can be used with a NEMA style type S starter.
This is only available for size 00, size 0, and size 1 starters.

Replacement/Stand Alone Adaptor Bracket Only  (direct repl for any Size 00,0,1 open or enclosed Type S starter using a NEMA melting alloy, bimetallic or SSOLR relay):
2 Pole (for single phase applications) = 9065SADR751
3 Pole (for three phase applications) = 9065SADR75

Keywords: IEC, bimetal, overload relay, starter, form, 8536SA, 8536SB, 8536SC

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings