Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the 9065 type SF solid state overload relays mount to an 8536 type S starter?

Issue:
Mount a 9065 type SF solid state overload relay to an 8536 type S starter?


Product Line:
NEMA Contactors and Starters


Environment:
8536 Type S Starters


Cause:
Can the 9065 type SF solid state overload relays mount to an 8536 type S starter?


Resolution:
The solid state overload relays from size 00 to size 1 are the same for separate mounting and replacement/retrofit mounting; size 2 and above use the type ST instead of the type SF and these devices are designed for separate mounting, not for mounting to a starter. The 9065 type ST should be used to mount to size 2 and above starters.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings