Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the ratings of the auxiliary switch, bell alarm, and shunt trip for EDB circuit breakers?

Issue:
Ratings of the auxiliary switch, bell alarm, and shunt trip for EDB circuit breakers

Product Line:
Circuit Breakers

Resolution:
Maximum currents and voltage are as follows:
The shunt trip max burden is 288 VA
Aux contact rating: 10 Amps @ 120 Vac
Bell alarm contact rating: 7 Amps @ 120 Vac

Schneider Electric Canada

Attachment(s)
48840-097-02.pdf [127.98 KB]
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings