Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement overload relay for an 8536SB starter?
Issue:
What is the part number for a replacement overload relay for an 8536SB starter?

Product Line:
All Schneider Electric products

Environment:
Products sold and used in the United States

Cause:
Need to replace the overload relay on a class 8536 type SB size 0 starter

Resolution:
The replacement overload relay depends upon the device used and any Forms originally ordered. The following outlines the replacement parts:

Two pole starter with melting alloy (no overload form), 9065SDO4.
Three pole starter with melting alloy (no overload form), 9065SDO5.
Overload relay Form B, 9065SDO6B.
Overload relay Form B1, 9065SDO5B1.
Overload relay Form B2, 9065SDO6B2.
Overload relay Form H10, 9065SS010.
Overload relay Form H109, 9065SSC10.
Overload relay Form H20, 9065SS020.
Overload relay Form H209, 9065SSC20.
Overload relay Form H30, 9065SF020.
Overload relay Form H308, 9065SFB20.
Overload relay Form H309, 9065SFC20.
Note: Starters with ``H`` Forms cannot be used on single phase applications for series A-E overload blocks, series F on can be used on single phase applications.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings