Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the operating ambient temperature for Square D panelboards?
Issue:
Operating ambient temperature for Square D panelboards

Product Line:
Square D Panelboards

Environment:
Application

Cause:
Panelboard location

Resolution:
Square D Panelboards are designed to operate within an ambient of 10 - 40 degrees Celsius (50 - 104 degrees Fahrenheit).

This means that any temperature below 10 degrees C will dictate the need for panelboard space heaters (with thermostat), and any temperature above 40 degrees C would require the equipment to be placed into a temperature controlled space to ensure the 40 degree C maximum temperature is not exceeded. An example would be if the panelboard interior is installed into any of our WP Nema 3R enclosures, and it is placed where direct sunlight can hit it.

If the ambient temperature approaches 80 degrees F, Consideration would need to be addressed concerning exceeding 40 Deg C /104 Deg F due to solar affect

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings