Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the pocket tester S434206 features?
Issue:
What are the pocket tester S434206 features?

Product Line:
Circuit breakers accessories

Resolution:
The pocket tester runs off of two alkaline AA batteries and does the following:
1- Powers up the trip unit on the breaker, lights the "Ready" LED, and allows settings to be made via the keypad
2- Provides thermal imaging inhibit functions for primary injection testing (NOTE: does NOT provide ground fault inhibit function)
3- Flashlight function

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings