Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are ALL the Canadian general duty, heavy duty, and double throw safety switches CSA certified?
Issue:
Product Design Features

Product Line:
Safety Switches

Resolution:
If the catalog number is shown in the current Canadian Digest and there is NO footnote stating otherwise, then YES, all the Canadian safety switches will be CSA Certified.
NOTE:
Most of the Canadian safety switch catalog numbers will begin with a prefix 'C', BUT there are some that will be the same catalog number as the US, UL listed catalog number. For example, the 800 and 1200 A, along with the 4 pole and 6 pole heavy duty and many of the double throw safety switches.
ON-LINE CANADIAN DIGEST LINK

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings