Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the JDCMH mounting kit accept 2 pole J frame breakers?
Issue:
JDCMH characteristics

Product Line:
Panelboards

Resolution:
Yes, the JDCMH will accept 2 pole J-frame breakers since the 2 and 3 pole J-frame breakers are the same dimensions.
Conditions for the JDCMH are:
- CDP interior with flat or extruded bus
- Cannot mount an old breaker back to back with new PowerpacT breaker

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings