Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement for the Compact NSJ or Powerpact D frame breaker?
Environment:
Compact NSJ and Powerpact D frame circuit breakers

Resolution:
The suggested replacement is the PowerPacT L frame.
Note: if replacing a plug-in or drawout version (N or D in the termination digit), the PowerPacT L still uses the same plug-in base and drawout cradle, so the L frame will fit right in. If an existing plug-in base or cradle is being used, use suffix HJ00 to get an L frame breaker only. Without the suffix, the breaker and base/cradle come as standard.

When crossing D frame circuit breakers, please note that all 400 A and below D frame breakers are 100% rated. The 600 A D frame breakers are standard (80%) rated only.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings