Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement 3 pole starter for an 8810SCO1?
Issue:
Checking on the replacement 3 pole starter for an 8810SCO1.

Product Line:
NEMA Contactors and Starters

Environment:
8810 Two-Speed Starters

Resolution:
The replacement parts consist of the following:
5P Device / Starter Components = 8536SCO3* (3P Starter) + 9999SB9 (2P NO Power Pole)
3P Device / Starter Complete = 8536SCO3*
Electrical Interlocks (only the internal NO is supplied with 8502 or 8536 replacement)
Internal: NO = 9999SX11 and NC = 9999SX12
External: NO = 9999SX6 and NC = 9999SX7


*add the appropriate voltage code to complete the part number

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings