What are the catalog numbers for the clear plastic covers over Micrologic trip units on the H, J, and L frame breakers?
Issue:
Cover for trip unit is broken or lost
Product Line:
Powerpact H J L
Resolution:
Cover for trip unit is broken or lost
Product Line:
Powerpact H J L
Resolution:
| Trip Unit | Breaker Suffix | Cover P/N |
|---|---|---|
| Micrologic 2.x and 3.x | M38X, U31X, U33X | S429481 |
| Micrologic 5.x and 6.x | U43X, U44X, U53X, U54X | S429478 |
| Trip Unit | Breaker Suffix | Cover P/N |
|---|---|---|
| Micrologic 2.x and 3.x | M38X, U31X, U33X | S432461 |
| Micrologic 5.x and 6.x | U43X, U44X, U53X, U54X | S432459 |
Released for: Schneider Electric Canada