Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot change output register label (all labels used) in Designer(PME)

Issue:
Saving a custom template, gives 'could not change label' or 'all labels used' message.

Visual of custom label error in PME Designer

Product Line:

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

ION Meter(s)

Environment:
Designer

Cause:
Pasting a large custom framework in a meter in which the output register labels have been modified from the default for a large number of modules.

Resolution:
There is a limit to the number of modules whose output register label can be customized from the default. The only workaround is to modify an output register custom label back to a default label in a module that does not necessarily need a custom label. This will provide an unused label which can be used in any other module's output register.

Recommendation:

If you are using an older version of PME, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo-psup@se.com

Support details

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings