Issue:
When selecting a Schneider Electric TeSys U IEC Style Simple Motor Starter for a new installation, consider using the resources listed below.
Product Line:
TeSys U Simple Motor Starter
Environment:
All TeSys U IEC Motor Starters
Cause:
The TeSys U consists of a control unit snapped in current limiter, predictive maintenance options, and communication options. To define the system requirements in order to select the appropriate device and accessories that will accomplish the task in question, please consider these parameters:
- Power Base Amp rating
- Control Unit current setting range
- Control circuit voltage code
- Associated auxiliary contacts
- Communications module.
Resolution:
Consider the following available resources:
(1) Our Online Digest. Please refer to Chapter 18
http://www.digestplus-us.schneider-electric.com/
(2) Further assistance is available from a local authorized Schneider Electric Distributor, using our Distributor Locator at the below link:
www.se.com/us/sites/us/en/support/distributor-locator/power-industry-locator.page
Released for: Schneider Electric Canada